EtherCAT Motion Bus Concepts
To exchange data between the controller (master) and the devices (slaves), the KAS Kollmorgen Automation Suite Runtime In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
In KAS, runtime refers to the virtual machine that manage the program written in a computer language while it is running. relies on
In cyclic mode, a single frame In networking dialect, a message is called a frame. containing the data of all slaves (input and output) travels along all slaves and goes back to the master. Data is read and/or written on the fly by each slave.
The slave device input and output data definitions are:
- Outputs are written by the master and read by the slave device.
- Inputs are written by the slave device and read by the master.
EtherCAT Process Image
This cyclic frame is called the EtherCAT Process Image.
- It contains the Process Data, which is defined during network initialization.
- The cyclic data is grouped in predefined blocks called Process Data Objects or PDO Process Data Opjects - A type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices..
- See these sections for more information about EtherCAT.
-
-
PDOs contain real-time cyclic data which is deterministic.
Non-cyclic data is not deterministic and is defined by Service Data Objects (ScDO).
References
- EtherCAT Specification V1.0 - see http://www.ethercat.org in the Member Area - Downloads.
- Büttner, H.; Janssen, D.; Rostan, M. (2003), EtherCAT - the Ethernet fieldbus, (PDF), PC Personal Computer Control Magazine 3: 14-19.